This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device For application

Other Parts Discussed in Thread: DRV8842

Hello Team,

Are there any motor driver ICs that are military-rated that can also switch the motor direction based on input?I have seen a few drivers that just turn the motor on and off, but do not swap directions when needed.

Regards,

Renan 

  • Hi Renan,

    There is the DRV8843-EP which is an enhanced package version of the DRV8842. It can support defense, aerospace, and medical applications. It also supports military temperature range (-55C to 125C). Unfortunately, this device is out of stock at the moment.