Hello, Team,
Our customer is currently evaluating DRV8832-Q1.
The configurations are:
- VCC: 3V
- VREF-VSET resistor: 53kΩ (from datasheet p7)
- VSET-GND resistor: 75kΩ (from datasheet p7)
- ISENSE-GND resistor: 0.2Ω (calculated from R ISENSE=200mV/1000mV)
- FAULTn : NC
In the above setting:
- IN1=0, IN2 = 0 -> IN1 = 1, IN2 = 0 : it rotates, but stops
- IN1=0, IN2 = 0 -> IN1 = 0, IN2 = 1 : it rotates in inverse, but stops
Customer wants the motor to keep rotating, but it does not current configuration.
What are they missing?