Other Parts Discussed in Thread: DRV110,
We are using three Staiger spider microvalve VA 204-508 24V with three DRV120A valve drivers. I have a Peak current set of 100mA and a hold current of 50mA.
Rpeak - 162k
Rhold - 133k
Rosc - 160k (25kHz)
Ckeep - 10uF (750ms)
The peak current I am seeing is 63mA which is okay as this is the full current for the valve.
The hold current I am getting is about 36mA, but has been as low as 30mA on one device on one board which resulted in the valve not holding open when under pressure.
Is there something incorrect in the datasheet w.r.t. to the calculations? Or is this within the expected tolerance?
I have also been testing with a resistive load equivalent to the valve of 360R, this is showing an average current of ~6mA with a low mark space ratio on the output of the FET.
I've also notice that the data sheet refers to a SENSE pin, (which doesn't exist) and the Internal RSense value is not specified.