Hello Ti Team,
I am developing a driver board for the BLDC Motor and Brushed DC Motor.
My Motor working voltage =+24V and Max Current rating is 1.2 A.
For these i selected DRV8343H IC as i want to work in Hardware configuration.
The external MOSFET , I am using is SIZ240DT-T1-GE3.
In datasheet, I am not able to find, how to calculate the Current Sense Resistor as you mention the low side driver.
As mention below image where i have to connect the VRef? (Should I connect to VM?)
Thanks and Regards,
Uday.