Instruction: DRV8343 drive chip write to close 6 MOS tubes via C1 (address 0x04).
Result: The MOS tube is not turned off, but the instruction is written in, as shown in the figure below:


NOTE: a. The 6xPWM mode is currently used.
b. The voltage at the MOS tube is still the output voltage of the PWM after the shutdown instruction is written.
The customer would like to know the way to close the MOS tubes. Thanks!
Best Regards.
Cherry Zhou