Hello,
My customer is wondering if they set the device up to have a 3A peak current for 4ms, and then want to switch to a 0.5A hold current, will the device make the switch even if the peak current hasn't been reached? Looking at the datasheet it doesn't seem to indicate anywhere the that switchover from TKEEP is related to anything other than teh capacitor value on the KEEP pin, but I want to clarify this.
Thanks,
John