Part Number: DRV8718-Q1
Dear expert,
Could you share me Example source code for DRV8718 and DRV8909?
Great thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DRV8718-Q1
Dear expert,
Could you share me Example source code for DRV8718 and DRV8909?
Great thanks
Hi,
DRV8718 does not have example source code, because device can wake up and functions with default basically. Then hardware interface such as nSLEEP/INx will be used to start motor operation. Customer can adjust each parameters via SPI based on customer's application.
DRV8909 is not available part name. If you meant as DRV8908, my answer is same as DRV8718.
regards
Shinya Morita
Ryan,
We do have example code for the EVM. You can find in the tool folder. This is for MSP430 MCU.
https://www.ti.com/tool/DRV8718S-Q1EVM
Regards,
Ryan