This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: DRV8323

Part Number: DRV8323


In our design we are using DRV8323HRTAR   for driving motor.

The Motor stall current is 13A.

Hence i need to set VDS cut-off at 13A. The external drive MOSFET RDS on value is 22.5mohm.

To cut-off at 13A, i need to set at V=13*22.5mohm= 0.29V

For hardware device i am using, i could find only 6 levels to set for VDS cut-off.

After 0.26 it is 0.6.

Is there provision to set in between 0.6 and  0.26(exactly at 0.29V).

Will this work with a higher  pull down resistor (say 80K) , so that we can set at 0.29V exactly.