Other Parts Discussed in Thread: DRV8353
Hello,
I am driving a 48V BLDC motor with 32V using the example code from the Instaspin Lab 5b, on Code Composer studio. I am bypassing motor identification.
When I increase the speed of the motor the fault LED on the DRV8353 board turns on. However, when I stop the motor, the fault LED turns off. It is a GDF fault. I tried changing the IDRIVE and the time settings like the datasheet indicates to no avail.
I measured the low and high side Mosfet signals. The GHB (Yellow) signal has erratic behavior, not following the INHB (purple) signal, as can be seen in the picture below. The other Mosfet signals are fine. Could you try and help me troubleshoot this issue?