Other Parts Discussed in Thread: DRV8312, DRV8353
Hello Guys,
Good day.
Our customer has the following application and wants to confirm if AVDD of DRV8302 can be use in such manner:
"I need to use drv8302 together with drv8312 in a project.
In the project, MCU (3.3V), drv8302 and drv8312 will be used together.
The drv8302's buck converter will feed the MCU, providing 3.3V energy.
drv8312 also needs 12V.
Main supply ie Pvdd = 48V;
Drv8302 has an internal regulator to feed the gate pins. But not in drv8312.
Can I use the Avdd pin of the drv8302 to feed the Gvdd pin of the drv8312?
In summary, can the energy in the Avdd pin of the drv8302 also feed the Gvdd pin of the drv8312?
Two different motors will be driven, this is exactly why drv8302 and drv8312 are used at the same time.
I think the drv8312 needs two separate power supplies."
Thanks and regards,
Art