This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV10975: How to control the speed bu IIC

Part Number: DRV10975
Other Parts Discussed in Thread: DRV10987,

Hi:

    I  can used the DRV10975EVB to control the motor speed by IIC .But it do not work in my appylication.

Following is my soft initialization:

1. 0X03 write 0X40 (enable EEPROM config)

2. EEPROM config

  0X20:0X6C

  0X21:0X07

  0X22:0X2C

  0X23:0X00

  0X24:0X00

  0X25:0XD1

  0X26:0XE4

  0X27:0XFC

  0X28:0X53

  0X29:0XD8

  0X2A:0X09

  0X2B:0X4E

3.0X01 write 0X80 (IIC  Speed contrl oveRide )

4.0X01 write 0X80

   0x00 write 0x96 (write the speed value)

When get  into  the colosed loop,the Speed is 9360RPM about .And I change the start Speed Value conmand ,when get into the closed loop ,the speed is still 9360RPM about.But,When use the DRV10975EVB ,the same speed value conmand,Speed is 7280RPM.So i think maybe some mistake in my applicaiton ,I can't debug to the speed what I want  .Please help me to check it,Also help to check the EEPROM Config whether it is suitable to the Motor,Thanks!

Attachment is my SCH and Motor Spec

Best Regards!

Chris