I'm designing a board that will probably have an efficient regulated 5V supply, and will certainly have regulated 3.3V. Can I apply 5V (or 3.3V if it's all I have) to the VREG pin and leave SW disconnected to reduce power loss?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm designing a board that will probably have an efficient regulated 5V supply, and will certainly have regulated 3.3V. Can I apply 5V (or 3.3V if it's all I have) to the VREG pin and leave SW disconnected to reduce power loss?
Hello John,
Thanks for your question. I have attached an image below for reference, but the logic core is powered from the 1.8V LDO which is powered via the Step-down regulator. For this reason we do not recommend connecting an external power supply to VREG pin as it may damage the device.
Best,
Isaac