I have made a custom board using DRV8305 and the board has been verified by Aaron Barrera
However, when I am using Lab 01b, everything works fine when I enable the system, but as soon as I put 1 in "gMotorVars.Flag_Run_Identify" the nFault is pulled low.
What is the dependency of following values on the value of shunt resistor, for the DRV8305 BOOST XL the shunt resistor value is 0.007 ohms and have following values, how should it be scaled for a shunt resist of 0.001 ohm?
#define USER_IQ_FULL_SCALE_CURRENT_A (24.0)
#define USER_ADC_FULL_SCALE_CURRENT_A (47.14)