Part Number: DRV8830
Hello,
In the datasheet of the IC in question (DRV8830) we have section 7.3.3, specifically bellow quoted paragraph which describes the driver behaviour during a stall event.
It is unclear to me though if the driver remains functional, thus pumping current into the DC motor, after the stall event is detected.
The last afirmation "Operation of the motor driver will continue." seems to indicate so, but does it refer to the driving stage (H-bridge) being automatically switched-off after stalling detection occurs?