I am afraid this is a rudimentary question.
Is it possible to control a pulse motor (stepping motor) using DRV8823?
Is there any way to control a pulse motor (stepping motor) using the DRV8823?
(I want to control two motors, two-phase bipolar.)
The PWM fixed frequency is 50kHz. Is it correct to recognize that the speed control is controlled by PWM?
I have the DRV8823EVM evaluation module.