Hello,
I have several questions on the DRV8343-Q1 data sheet.
- 1PWM_COM bit in IC1 Control register:
- Is the 1PWM_COM bit effective only in 1x PWM mode?
- In the other mode than the 1x PWM, is the default rectification setting is synchronous?
- 1PWM_DIR bit in IC1 Control register:
- Is the 1PWM_DIR bit effective only in 1x PWM mode?
- Equations (8) and (10) in the "9.2.1.2.2 IDRIVE Configuration" section:
- Is the equation (8) "IDRIVEP > Qgd × tr" correct? I suspect it must be "IDRIVEP > Qgd ÷ tr".
- Is the equation (10) "IDRIVEP = 12 nC / 1000 ns 14 mA" correct? I suspect it must be "IDRIVEP = 14 nC / 1000 ns = 14 mA".
- Accordingly, is the description above the equation (10) correct?
- "Use Equation 10 to calculate the value of IDRIVEP for a gate-to-drain charge of 14 nC and a rise time from 100 to 300 ns."
- EN_SHT_TST and EN_OLP bits in IC2 Control register:
- When should these bits activated? Right before performing these diagnostics?
Best regards,
Shinichi Yokota