Hi,
I would like to use DRV2510 driver for one coil motor.
The input signal including a DC, That means the during a 1 cycle of work there is time that the input is just a dc voltage.
Is this drive can drive a dc signal? is the driver output is stable when the input it's DC?
Thanks,
Avi