Hi there
I have a MCT8316ZTEVM and a EC60 flat BLDC-motor from maxon.
The motor has 7 pole pairs and a max rotating speed of 3700 rpm.
With the MCT8316ZTEVM the max rotating speed I can realize is 2000 rpm.
What do I have to do to get a rotating speed of 3700 rpm?
Best regards
Markus