This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV2605: DRV2605-Communicate

Part Number: DRV2605
Other Parts Discussed in Thread: EV2400, USB2ANY,

Hi Ti Team,

Does DRV2605 use EV2400 to communicate with PC?

  • Hi, 

    I assume that you have a DRV2605EVM-CT in which case the EVM uses a USB2ANY(https://www.ti.com/tool/USB2ANY) to connect with the PC/Haptic control console.

    section 7.1.1 of the haptic control console GUI users guide explains how to set this EVM up with the USB to any.

    the USB2ANY appears to be out of stock on TI.com, but I see that Digi key has several available

    I am not familiar with EV2400, but if you are able to use it as a generic I2C master it (arbitrary address/register writes etc.) then this could also be used to configure the DRV2605, however it likely wont work with HCC.

    Regards,

    Arthur