Hello,
I'm working with DRV3245Q-Q1 and from the documentation I don't understand clearly what happens when I lose a phase (e.g. open of motor phase):
- predriver set only a warning to uc? OR
- predriver 'switch off' all phases?
Can I still use the other 2 phases, to perform a simplify control of the motor, in case the driver detects the failure?
Also is it possible in case of internal failure?
Thanks in advance for all the support
Nicolò