This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8353: Replace DRV8353RHRGZT with DRV8350RHRGZT: pin 26

Part Number: DRV8353
Other Parts Discussed in Thread: DRV8350

Dear e2e team,

My customer is considering to replace the DRV8353RHRGZT with DRV8350RHRGZT.
Comparing the pin-out, these devices are compatible but the only problem seems the pin 26: in the case of DRV8353 it is connected to Vref but in the case of DRV8350 it's recommended to leave it floating or connect it to GND.

Do you think that should be any problem connecting pin 26 to +3V3?

Thanks,

Giorgia