Other Parts Discussed in Thread: DRV8301
Hello,
I am using a BOOSTXL-DRV8301 and I have a question regarding current measurement.
The characteristics of this board I use are as follows.
: support 6 - 24V and up to 100A RMS(14-A Peak)
However, if you look at the circuit diagram and description of this ( page. 7), the current measurement is scaled to +/- 16.5A.
Then, the current of +/- 16.5A can be input as a voltage of 0~1.65 ~3.3V through the current sense configuration, but can this board actually receive only +/-10A of current?
Can't I receive more than 10A current? up to 15A