Hi,
I just bought the DRV8332 to control a motor of 24V/10Amps.
I need help how to connect it to the motor and how to determine the required circuit configuration and the components values.
Please advise!
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The datasheet provides several application examples to help guide you.
http://focus.ti.com/lit/ds/symlink/drv8332.pdf
In addition to the datasheet, we recently released a complete motor kit....DRV8312-C2-Kit....that you can purchase to evaluate a DRV83xx in a 3-phase system. The DRV8312 is just a lower current version of the DRV8332. All the tools for the DRV8312 would also apply to the DRV8332.
http://focus.ti.com/docs/toolsw/folders/print/drv8312-c2-kit.html
The documentation for the kit above is available through the link below:
http://focus.ti.com/docs/toolsw/folders/print/controlsuite.html
I hope this helps!
Best Regards,
Ryan
Munish,
What is your intended use for a single phase motor? Are you talking about an Induction motor or a brushless DC motor? Also, why have you chosen single phase?
Thanks,
Matt