Hi team,
Issues:
1. when the motor is spinning, IN1 and IN2 inputs are high at the same time, causing the motor to brake, but the motor will not brake as expected. The FAULTn pin can detect that it is pulled low.
2. when the chip is in the initial state of IN1 and IN2 input high simultaneously, pull one of the pins low and the motor will not start. The motor can only be rotated by pulling one of the pins high when the initial state is IN1 and IN2 input low.
3. if the ISENSE pin is connected directly to ground, try to start the motor, the motor cannot start, and the FAULTn pin can detect that it is pulled low.
4. when the IN1, IN2 inputs are one high, one low, normally control the motor rotation, there is a certain probability that the motor will stop abnormally, test IN1 and IN 2 with an oscilloscope, the input does not change but OUT1, OUT2 no longer outputs the voltage. And this phenomenon only occurs in one direction of motor rotation, not in both directions where the motor may stop abnormally. When the motor stops abnormally, the FAULTn pin output may be low or may still be high-impedance.
Could you help check this case? Thanks.
Best Regards,
Cherry