Other Parts Discussed in Thread: TMS320F28069M, , DRV8323R, MOTORWARE, LAUNCHXL-F280049C, BOOSTXL-DRV8320RS, BOOSTXL-DRV8323RS, LAUNCHXL-F28069M
Hello,
TMS320F28069M on a TMDSCNCD28069MISO v0.4 on DRV8301-HC-EVM rev.D
We are looking forward to use InstaSpin FOC in our new product, all tests where good.
For this we also purchased many 80 pin TMS320F28069FPNT (the 80 pin FOC).
Though.... this nice driver on the eval Board the DRV8301, is now obsolete.
TI has one alternative (the DRV8323R) and some more are coming up in the market.
But....
Some drivers have SPI communication pins, and some don't. The DRV8301 does have SPI, and GPIO lines (GPIO24-27) of the MCU are dedicated for that
(as GPIO lines (GPIO16-19) are dedicated for the second SPI on board, but is not set up).
The Question: Does the code use SPI to talk to the driver, so we have to buy a driver with SPI on it, OR, the code does not talk to the driver so we can buy a driver with or without SPI on it?
Thank you