What's the releationship between the 2 stages charge pump?
Can we use the chagre pump to driver additional 3 MOSFETS for motor phase isolation? That means we would like to drive 9 MOSFETS, 6 ones for bridge and 3 ones for phase isolation.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What's the releationship between the 2 stages charge pump?
Can we use the chagre pump to driver additional 3 MOSFETS for motor phase isolation? That means we would like to drive 9 MOSFETS, 6 ones for bridge and 3 ones for phase isolation.
Hi Zhi,
The DRV3245-Q1 device uses a two-stage charge pump like mentioned. Here's some details below to explain the behavior:
Also, do you have access to the product datasheet?
For your comment about driving the additional 3 MOSFETs for motor phase isolation, are you going to be driving them through some external circuit connected to the gate-drive signals: GHx, GLx, SHx, etc?
Thanks and Best Regards,
Andrew
Thanks! I got the datasheet.
I would like to consult you about the value of Bootstrap Diode Current Limit.
And it's better if you could recommend the method to evaluate whether the GDU is enough to drive many MOSFETs at the same time.
Thanks in advance.
Hi Zhi,
I think for this DRV3245-Q1 device, there is no bootstrap diode (since it uses a charge-pump architecture instead to produce the needed gate-driver voltage for HS pre-driver)
The datasheet section you shared (9.2.2.1 External MOSFET Support) is the correct guideline for calculating the MOSFET switching capability under 'average' gate drive current conditions like mentioned.
Also, one more comment regarding the equation for average charge pump current capability:
Thanks and Best Regards,
Andrew