Hi,
I wish to consider the DRV3245-Q1 for an application where the supply voltage ranges from 12V to 28V. As this gate driver is rated max 45V, it is unsuitable for use at 28V due to the possibility of load-dump transients damaging the device.
Has anyone incorporated additional transient protection in the supply line to enable a lower-voltage gate driver (such as the DRV3245-Q1) to be used at higher voltages whilst ensuring it is safely protected from transients up to at least 60V?
Would the addition of TVS or similar devices on the input supply be sufficient?
Thank you in advance,
- Alan