Hello TI,
Hope all is well.
I'm using the DRV8832 in a new application. I've limited ISET to 1A using 0.2Ohms on the ISENSE pin to ground. VSET is set to 3.0V and 4.2V<VCC<3.0V. The motor consumes about 0.7A maximum but in-rush current can go as high as 1.5A in some situations.
Few questions:
1- Motor current at OUT1/2 is limited to 1A internally, however in the first page of the datasheet shows 1.3A peak to the motor, see picture below. What's the true maximum current that can be supplied to the motor?

2- Looking at the Iocp ratings, 3.0A<Iocp<1.3A, FAULTn is triggered when Iout>Iocp, is there a way to limit Iocp? To avoid FAULTn triggered because of in-rush current, it is desirable to set Iocp to 2.0A, is that possible?
3- Would an external 10uF capacitor on OUT1/2 (in parallel with motor), help on the in-rush current?
Look forward to your feedback.
Thanks