Other Parts Discussed in Thread: DRV8876, DRV8873, DRV8874, DRV8256
Hi TI,
We would like to use the DRV8412 in a 100% duty cycle operation and if possible we would like to avoid the min. 50ns pulse for the bootstrap capacitor charging. Would it be possible to use an external power supply tied to the BST_X pin instead of the bootstrap capacitor?
If this would be an option I have a few questions regarding the implementation:
- would the external bootstrap supply need to track the GVDD_X supply in order to maintain the boot voltage above the min. BST_UVP voltage (~7V)?
- a simpler implementation of the above would be a fixed voltage above the GVDD_X and maybe just some current limiting resistors on the BST_X pin? Would this be possible?
- or do you have any other suggestions for using the DRV8412 in 100% duty cycle mode?
Thank you,
Tilen