Other Parts Discussed in Thread: DRV8305
Please tell me what difference is between DRV8305NQPHPRQ1 and DRV8305NPHPR.
Our customer can't get DRV8305NQPHPRQ1.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Please tell me what difference is between DRV8305NQPHPRQ1 and DRV8305NPHPR.
Our customer can't get DRV8305NQPHPRQ1.
Hi Kura-san,
DRV8305NQPHPRQ1 is automotive grade 1 version of DRV8305, with VREG applied externally (internal VREG regulator and VREG_UV fault are disabled). DRV8305NPHPR is industrial version.
Thanks,
Aaron
Aaron-san
Thank you for your reply.
Does this mean that the difference between DRV8305NQPHPRQ1 and DRV8305NPHPR is only automotive qualification ?
Are the die and the package materials and wafer/assembly/test sites same ?
Hi Kura-san,
Will look into this and get you a response once I confirm a few details.
Best Regards,
Andrew
Hi Kura-san,
Following up on this item -
Quick question: What is your customer's application? Is it automotive?
From our database information, these two devices have:
Thanks and Best Regards,
Andrew
Hi Kura-san,
Also one more note: when you are selecting the Q1 vs non-Q1 substitute, please be sure to know the below key differences in the variants of the DRV8305x device family.
This mainly has to deal with the LDO voltage reference in 3 vs 5 vs N vs NE options.
|
Device |
DRV83053Q |
DRV83055Q |
DRV8305NQ |
DRV8305NE |
|
Ambient Temperature range (oC) |
-40 to 125 |
-40 to 125 |
-40 to 125 |
-40 to 150 |
|
LDO |
3.3 V / 50 mA |
5 V / 50 mA |
NO |
NO |
|
Overtemperature shutdown |
Yes |
Yes |
Yes |
NO |
Best Regards,
Andrew
Hi Kura-san,
Thanks for your answer on this!
I think the information above about Q1 (automotive) vs non-Q1 (industrial) should be helpful in your team's decision making of supply sourcing.
I'll send another message internally to our team to see if the application (power slide door) itself has any major concerns
Best Regards,
Andrew
Andrew-san
Thank you for your support.
We got following request from customer.
Do you have actual difference point list between DRV8305NQPHPRQ1 and DRV8305NPHPR and DRV8305NEPHPRQ1 ?
If yes, please send it to us.
Regards,
Kura
Hi Kura-san,
Please see the chart below - if we are purely considering N vs NE versions, then the difference should be the over-temperature shutdown functionality. Should have no major difference between industrial (non-Q1) and automotive (Q1) from a functionality point of view
|
Device |
DRV83053 |
DRV83055 |
DRV8305N |
DRV8305NE |
|
Ambient Temperature range (oC) |
-40 to 125 |
-40 to 125 |
-40 to 125 |
-40 to 150 |
|
LDO |
3.3 V / 50 mA |
5 V / 50 mA |
NO |
NO |
|
Overtemperature shutdown |
Yes |
Yes |
Yes |
NO |
Thanks and Best Regards,
Andrew
Hi Kura-san,
Will follow up on this today - need a bit of time to check the answer w/ the team
Best Regards,
Andrew
Hi Kura-san,
From my system records, these two devices (N vs NE) use different die inside.
For these two Q1 devices, the NE version has 'extended' temperature coverage (up to 150C) so I believe the production test coverage might be more for this NE version compared to the N version (up to 125C). Test coverage is probably similar, but may have different temperature guardbanding and production test limits implemented for screening devices.
Thanks and Best Regards,
Andrew
Andrew-san
Thank you for your support.
Even though the data sheet and function are the same.
We would like to know the reason why Die is different between N vs NE.
And We also would like to know the effect of replacing them.
Regards,
Hi Kura-san,
Between the N vs NE versions, records indicate that the die name is different - but they may have the same (or very similar design).
I am not too sure on the answer for that, and am not sure if I can share that publicly regardless -
From pin-to-pin replacement perspective of DRV8305NQPHPRQ1 vs DRV8305NEQPHPRQ1, TI motor drivers team's advice is that production test coverage is different. If your application requires 150C max operating range then NE is the only option - but if you only need 125C, you can use either N or NE interchangeably for normal operation.
Also note that the NE version specifically has over-temperature shutdown feature disabled by default, so if you are wanting to retain OTSD -> will have to configure that in the SPI settings for 'FLIP_OTSD' bit in Register map address 0x9
Best Regards,
Andrew