Hi
What is IPROPI output when the IPROPI1 and IPROPI2 are tied together and used in H-Bridge? Especially in High-side recirculation (brake) timing? the current in both MOS are the same amplitude but opposite direction, so is it cancelled out?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
What is IPROPI output when the IPROPI1 and IPROPI2 are tied together and used in H-Bridge? Especially in High-side recirculation (brake) timing? the current in both MOS are the same amplitude but opposite direction, so is it cancelled out?
Hi Takuma,
The IPROPIx is equal to the scaled down current flowing through the drain to source of the high-side FETs of the respective half H-bridge. Tying IPROPI1 and IPROPI2 together will result in the sum of the current through high side FETs of both H-bridges (HS1 and HS2). However, this is only true if the current is flowing from the drain to the source of both FETs. During high side re-circulation, only one FET will have current flowing from drain to source. so IPROPI (IPROPI1 + IRPOPI2) will only be equal to the current flowing one of the FETs.
I hope this answers your question.