This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] DRV2625: DRV26xx Reference Design

Part Number: DRV2625

Below you can find the basic application reference design for parts from the DRV260x and DRV262x Families

The only difference in reference design being that supply rails for the DRV262x series of parts has a range of 2.7V - 5.5V and does not accept PWM input at the IN/TRIG pin. EN is replaced by NRST on DRV262x

Recommended values: C(VDD)C(REG) = 1µF and R(PU) = 2.2kΩ for DRV260x and C(VDD) = C(REG) = 0.1µF and R(PU) = 2.2kΩ DRV262x

If IN/TRIG is not used you can tie to ground and on the DRV262x design NRST pin can be connected Directly to VDD if desired

LRA/ERM is recommended not to be below 8Ω and does not support below 4Ω

Note: DRV260xL version has supply rail range of 2V - 5.2V