Hi team,
Here's an issue from the customer may need your help:
The DRV8824 is used to drive a two-phase stepper motor using the VQFN package, which is a 0.2-mm to 0.3-mm pin width for OUTA and OUTB, so the PCB line width is limited to within 0.3-mm for PCB layout. While the motor set current is 1.8 A RMS and the PCB copper thickness is 0.5 oz, this current is used for a line width of 0.3 mm. Will this way have any bad impact and could you give some recommendations for layout?
Could you help resolve this case? Thanks.
Best Regards,
Cherry