Hi Team,
Good day! I am posting this in behalf of the customer. I have shared here below the full details of their inquiry.
I am using DRV8301 Kit, in which i have completed InstaSpin Motion and FOC Lab procedure for
1. Lab2a Motor ID from ROM
2. Lab05c for InstaSpin Motion Inertia ID
3 Now i am stuck in Lab12a Procedure where in
gMotorVars.Flag_enableSys value overrides to 0 even after changing it 1 '\0x01'
(gMotorVars.Flag_Run_Identify sets to 1 on changing it from 0 to 1 value but issue with gMotorVars.Flag_enableSys )
I have done all the prerequisites required for this lab, also checked user.h file declarations, checked Encode, A, B, I signal connections and Motor phases connections with the board.

Previously build Labs 2a and 5c worked perfectly fine,
I am doing this procedure as ultimately my application is same as Lab13a Tuning SpinTAC Position Control and it is mentioned there in prerequisites of this lab to follow Lab12a procedure,
Kindly suggest appropriated actions in this regards,
Jonathan