I need to identify good alternates for the following ST parts:
High side: VN5050JTR-E
Low side: VND7NV04TE-E
I don't care what package, but the ratings should be as close as possible.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Mike,
Thank you for your post.
A couple of questions:
1) I noticed these are automotive parts with load dump specifications, etc. Is this for an automotive application where Q100 qualification is required?
2) What is the load current in your system? Can you tell me a little more about what you are driving....motor type? We have some integrated parts that include the power FETs that might be better suited as a complete solution. If I know what current you need, I can make some suggestions for you.
3) Voltage range in your system that must be supported?
Regards,
Ryan
Ryan,
Thanks for the quick reply - I failed to provide some of the details. No auto or Q100 qual is required. A critical requirement is ability to control each driver independently. Here's the full requirements list:
Mike
Mike,
Take a look at the DRV8412. You can configure it in a Parallel BTL mode and cut the Rdson down to ~60mohm. Device is surface-mount with exposed thermal pad on the bottom for heat sinking into copper in the board.
It has a PWM input. In the PBTL mode, the OUTA/OUTB outputs will track PWM_A input and OUTC/OUTD will track PWM_B input. Deadtime control is built-in.
http://focus.ti.com/docs/prod/folders/print/drv8412.html
Regards,
Ryan
Ryan,
This is great! What a beast of a part! One other thing I'd like to ask, though. Is there a similar 2-chip solution with separate Hi & Low side drivers? This is not actually for a motor, but the motor driver parts work well. Physically separating the 2 sides may give me a little more flexibility.
Thanks.
Mike,
We will be releasing a "pre-driver" part in June that will allow independent control of external FETs. The part number is DRV8301. It is in preview state now. If you post your email, I can send you a preliminary datasheet.
Regards,
Ryan