We are operating 2 stepper motor with single DRV8711 driver IC. Motor is taking 1.3 Ampere of current after making changes in parameters suitable with our requirement. But after rotating 2 or 3 round motor driving ic is giving undervoltage and predriver fault. Though we are moving motor without any load. Is there any specific parameters we have to set ?