Part Number: DRV8244-Q1
Hi team,
I couldn't find information of the maximum current from IPROP pin.
The EC table shows the current scaling factor of IPROP function is tested up to 8.3A.
I don't think 8.3A / A = 8.3A / 4570(HVSSOP) = 1.8mA is a acceptable maximum current from IPROP pin because this device can handle 21A.
Could you please check the maximum current from IPROP pin?
Customer wants to set the ITRIP function at 15A. So, IPROP current < 8.3A is not enough for it.
Regards,
Saito