Hi,
I want to rotate a 1-pole BLDC motor at 10,000 rpm±3rpm.
Is it possible to store MAX_SPEED_REGISTOR = 1,000(0x03E8)?
In that state, If I instruct any Duty_CMD to Maximum, will it rotate at 10,000rpm?
I would like to try the analog input of SPEED control,
but I think that the rotation speed may change due to the error of the indicated voltage,
so I wanted to confirm this method.
Best regards,