Hello ,
I'm using the DRV8842. In the "Typical Application part given in the datasheet, there is a equation for
calculating I_Trip depending on VREF and R_Sense. Is I_Trip = 1.5A by one directional current or
is the bidirectional current range from -0.75 to +0.75 A.
I want a small R_Sense and the motor maximum current should be +/-1A by 100%.
INA240A2:
Additional i'm also confused by the given equation for calculating R_Sense for the INA240A2.
Im using the differential measurement Figure 8-8. Vs = 5V, and the internal reference for the ADC by the microcontroller is 2.56V.
So i'm also strugggeling what to use as V_Ref... The Internal 2.56, two times 2.56V
cause im measuring birectional or die reference voltage given by the resistor divider?
As the maximum Current i want to use -/+ 1A, so a difference from 2A. What is my I_max... is it 1A or is it 2A?
Could you please help me choosing the right values...
Thank you very much!
F.Kamm