Other Parts Discussed in Thread: DRV8243-Q1, DRV8244-Q1
We are considering a system that can drive a proportional solenoid without using a microcomputer.
I would like to control the current with a resistor, etc., but please tell me a candidate for a motor driver.
In addition to the above requirements, the conditions for the motor driver to satisfy the system characteristics are as follows.
Up to 1.3A current
Voltage is steady at 12V, maximum is about 24V.
Ultimately aiming for mass production of about 3000 / month.
Satou