Hello,
How should I deal with DRV8343-Q1's INx/ILx/GHx/GLx/SHx/DLx/SLx pins when they are not used?
Best regards,
Shinichi Yokota
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
How should I deal with DRV8343-Q1's INx/ILx/GHx/GLx/SHx/DLx/SLx pins when they are not used?
Best regards,
Shinichi Yokota
Hi Yokota-san,
When a 1/2 bridge is disabled:
1) INHx/INLx - tie to GND or float
2) Tie GHx to SHx
3) Tie DLx, GLx, and SLx together
Tying INHx/INLx to GND or floating will keep inputs low. Keeping inputs low will disable VDS overcurrent monitoring because it is active when inputs are high.
VGS monitoring is always active, and it will expect VGS to be "off" depending on state of the input pins. Since inputs will always be 0, VGS should always be 0V, so tying gate to source for each gate driver output is recommended.
Thanks,
Aaron
Aaron-san,
Thanks for your feedback.
When a 1/2 bridge is disabled:
How about the case when the independent half-bridge mode is enabled?
Best regards,
Shinichi Yokota
Yokota-san,
What I meant is if you are not using the half bridge, above is how you deal with the unused pins. This will be okay no matter which mode the DRV8343-Q1 is using, including independent 1/2 bridge mode, because the inputs will be tied to GND and VGS voltages will always remain 0V.
Thanks,
Aaron
Aaron-san,
Now I understand it. Please let me rephrase it. Regardless of the PWM mode, the above is how I must deal with unused pins of a half-bridge that is not used.
Best regards,
Shinichi Yokota