Part Number: DRV8424EVM
Hi,
I have a question related with the current regulation.
This is my actual driver configuration:
- 1/16 Microsteps
- Smart tune dynamic decay and Smart tune ripple control (both have been tested)
- Toff = 16us
- Running Current = 800mA
- Speed = 300rpm
I have used two different stepper Motors:
- 29QQ Peristaltic Pump from Boxer pumps (200 steps per rev)
- Minebea 17PM-K443BNVA1637 (200 steps per rev)
I have measured the current with this configuration using a Shunt (2A-200mV), and the current has the following waveform for the 29QQ Stepper Motor without load:

With the same configuration using the Minebea 17PM stepper motor with a small load, the current waveform is the following:

In the second motor is possible to appreciate that the current has no sinusoidal waveform. Why is this happening?. I have read in the following document https://www.tij.co.jp/jp/lit/ml/slyp742/slyp742.pdf?ts=1644397542933&ref_url=https%253A%252F%252Fwww.google.com%252F that using the Smart ripple control the driver maintains sinusoidal current waveform at any speed. But I don´t see that in my measurements with the second motor.
Please could you give me an explanation why the sinusoidal current waveform is not maintained?
Thank you very much in advance
Best Regards