This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8889-Q1: How can we change it to improve the recognition accuracy

Part Number: DRV8889-Q1

In the process of using drv8889-q1, Turn left and right the feedback TRQ_COUNT is not same。 The following is the configuration content of drv8889. How can we change it to improve the recognition accuracy.

Ctrl3 register
MICROSTEP_ MODE :STEP_ 1_ four
SPI_ STEP : 1
SPI_ DIR :1

Ctrl1 register
TRQ_ DAC:CURRENT_ 87_ POINT_ 5_ PERSENTS

Ctrl2 register
TOFF:1
DECAY:SMART_ TUNE_ RIPPLE_ CONTROL

Ctrl5 register
STL_ REP :0
EN_ STL:1
STL_ LRN:0

Ctrl6 register
STALL_ TH :14

Ctrl4 register
EN_ OL:1
Judge by reading the feedback ctlr7 torque value in real time. When there is no locked rotor and the voltage is 13V, the value of TRQ_COUNT is 0x1f, and when locked rotor is detected, the torque value is about 0x0c. Then judge the locked rotor according to the time when the torque value appears.

  • Hi,

    Thank you for your interest in DRV8889-Q1.  This device has stall detection threshold settings. So picking up different threshold by direction could help.

     

    Changing microstep_mode to 1/16, 1/32 ... more "microstep" may help.

    regards

    Shinya Morita