Hello,
DRV8343-Q1 has two types of calibration for the current sense amplifiers - manual calibration and automatic one. I'd like to ask some questions about this function.
- Are the specs of the CSA's "VOFF - Input offset error" the ones after the automatic calibration?
- Is it correct to understand that the manual calibration requires voltage measurement at SOx pins?
- And then, the system must store the value and use it to offset the CSA's VOFF?
- If the answer to the above question is yes, I guess a residual input offset error depends on the measurement error. But, if ideally the measurement error is zero, how much can the residual input offset error be practically?
Best regards,
Shinichi Yokota