This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8323: Write the control registers using SPI communication.

Part Number: DRV8323

HI. experts.

I am using a DRV8323s to control a motor. I wonder what would happen if we continued reading and writing to the DRV8323s' control registers.

1. Is there any problem if I keep writing the same value to the control register?

2. Is there any problem if I change the new value in the control register and write it continuously?

I wonder if the control register of the DRV8323s has a lifespan depending on the number of writes.

Thanks for the reply.