This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MCF8316A: Is MCF8316A capable of driving 120W BLDC? 24v 5A motor.

Part Number: MCF8316A
Other Parts Discussed in Thread: DRV8316

Hi team,

Here's an issue from the customer may need your help:

Is MCF8316A capable of driving 120W BLDC?

The customer are using a motor from maxon. The power supply is 24V,  the current could be up to 5A,  That will be 120W power consumption on the MOTOR.

The mosfet inside the MCF8316A has inner resistance about 95m ohm, the energy  on that  will be 5*5*95 *2 = 50mW。  

The customer is wondering the MCF8316A can stand with taht, is that correct?

Could you help check this case? Thanks.

Best Regards,

Cherry