Other Parts Discussed in Thread: DRV8425
Hi,
Customer is designing a drive stepper motor and have following question regarding this. Please see details below.
"I am design a circuit to drive stepper motor using DRV8425PRGER, there is no application circuit for stepper motor. I do find DRV8425RGER datasheet for stepper motor with different pin definition. My questions are:
Can I use DRV8425PRGER to drive stepper motor? If yes, how the pin should be redefined (for example, ENABLE, DIR, microstep definition)
On page 32, there is a example of stepper motor driver circuit. Yet I need more detailed information how to set the microstep, which pin is used to control step, direction and etc. Most of datasheet is about drive BDC motor. Any setting to select BDC or stepper motor since the pin definition are different."
Regards,
Maynard