Other Parts Discussed in Thread: DRV8805
We have gone through the previous issues with DRV8805 EVM board and as per updated suggestions, we have connected the hybrid motor winding as
OUT1 : A+ ; OUT3:A-
OUT2: B+ ; OUT4: B-
COMM (Both) : VCLAMP
Our motor works from 12V DC to 24 VDC and consumes max current 2A.
Within 10 min my motor as well as IC heats up and it toggles between nFault high-low.
Kindly suggest the solution.