Part Number: DRV8884
Other Parts Discussed in Thread: DRV8886
Dear Sir,
I have fixed mode of operation of IOs of DRV8884 like TRQ, M1/M0, DECAY.
Details are as below.
1) TRQ, M1 - need to be logic low.
2) M0 - need to be logic high.
3) DECAY - 2.9 (slow decay for both increase/decrease steps)
Query is as below:
as per datasheet, M0 & TRQ pin is TRI-LEVEL Input pins; DECAY is QUAD-LEVEL input pin; M1 is LOGIC-LEVEL input.
Can I connect TRQ, M1 pins directly to ground OR I have to use some kind of external pull down resistor to make them logic low.
Can I connect M0,DECAY pins directly to DVDD pin of DRV8884 IC OR I should use some external series resistor while connecting to DVDD pin OR I should use external logic supply voltage instead of DVDD pin.
Regards,
Jigar