Hi team,
Here's an issue from the customer may need your help:
When the DRV10983 PWM control motor speed is applied, the fan does not start when 1% to 2% of the output input PWM controls the speed. Can only spin up at 100% Duty. Could you help check this case? Thanks.
Best Regards,
Cherry